i.MX 8X SCFW RTC IRQ Enable/Check Status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8X SCFW RTC IRQ Enable/Check Status

ソリューションへジャンプ
1,927件の閲覧回数
petar_petrov
Contributor II

Hello,

I would like to know which resource needs to be used when enabling the internal RTC's IRQ and checking its status? Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? Thank you in advance!

Best regards,

Petar

ラベル(1)
0 件の賞賛
返信
1 解決策
1,923件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Petar

 

> Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? 

 

it is SC_R_SNVS

 

Best regards
igor

元の投稿で解決策を見る

1 返信
1,924件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Petar

 

> Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? 

 

it is SC_R_SNVS

 

Best regards
igor