i.MX 8X SCFW RTC IRQ Enable/Check Status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8X SCFW RTC IRQ Enable/Check Status

Jump to solution
1,921 Views
petar_petrov
Contributor II

Hello,

I would like to know which resource needs to be used when enabling the internal RTC's IRQ and checking its status? Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? Thank you in advance!

Best regards,

Petar

0 Kudos
Reply
1 Solution
1,917 Views
igorpadykov
NXP Employee
NXP Employee

Hi Petar

 

> Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? 

 

it is SC_R_SNVS

 

Best regards
igor

View solution in original post

1 Reply
1,918 Views
igorpadykov
NXP Employee
NXP Employee

Hi Petar

 

> Should it be SC_R_SYSTEM or SC_R_SNVS (since that's where the RTC is located)? 

 

it is SC_R_SNVS

 

Best regards
igor