i.MX 8QM GPIO interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8QM GPIO interrupt

888件の閲覧回数
jens0501
Contributor II

Hello,

I am working on a project that uses the spear-mx8 board on a VAR-SP8Customboard. I have Linux running on the Cortex A cores and I am able to run some bare metal C code on the cortex M4 co-processors using the MCUXpresso SDK.

Now I want to configure a GPIO pin as input and use this pin to trigger an interrupt in the M4. I have seen examples of interrupts with timers, but I am unable to find some example or even some good documentation. Has anyone already used a GPIO as an interrupt on the cortex M4 or is there some documentation about this?

Thanks

ラベル(1)
0 件の賞賛
返信
0 返答(返信)