i.MX 8MQuad Evaluation kit boot-up issue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi,
Currently, I have working on i.MX 8M Quad Evaluation Kit. I have create one layer and add new machine in yocto. Now I try to flash evk board using below command.
sudo ./uuu -b emmc_all imx-boot-<machine>-sd.bin-flash_evk < custom bz2 image>
Output:
Success 1 Failure 0
uuu Flashing Log:
1:2>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:2>Okay (0.02s)
1:2>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:2>Okay (0.589s)
1:2>Start Cmd:FB: ucmd mmc dev ${emmc_dev}
1:2>Okay (0.213s)
1:2>Start Cmd:FB: flash -raw2sparse all /home/neel75/Downloads/LF_v5.4.y-1.0.0_images_MX8MQEVK/imx-image-full-imx8mqevk.sdcard
100%1:2>Okay (542.1s)
1:2>Start Cmd:FB: flash bootloader /home/neel75/Downloads/LF_v5.4.y-1.0.0_images_MX8MQEVK/imx-boot-imx8mqevk-sd.bin-flash_evk
0x400000001:2>Okay (0.422s)
1:2>Start Cmd:FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
1:2>Okay (0.011s)
1:2>Start Cmd:FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
1:2>Okay (0.013s)
1:2>Start Cmd:FB: done
1:2>Okay (0s)
Flashing Log on UART:
downloading of 1487560 bytes finished
request 00000000fdccb800 was not queued to ep1in-bulk
writing to partition 'bootloader'
Initializing 'bootloader'
switch to partitions #1, OK
mmc0(part 1) is current device
Writing 'bootloader'
MMC write: dev # 0, block # 66, count 2906 ... 2906 blocks written: OK
Writing 'bootloader' DONE!
request 00000000fdccb800 was not queued to ep1in-bulk
Detect USB boot. Will enter fastboot mode!
request 00000000fdccb800 was not queued to ep1in-bulk
Detect USB boot. Will enter fastboot mode!
request 00000000fdccb800 was not queued to ep1in-bulk
Observation:
1. Evk not boot-up in internal boot mode
2. I have flashed pribuilt image in evk but not boot-up in internal boot mode.
Question:
Please give the suggestion for this issue.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Which version of BSP are you using? Are you using the demo images or images you build yourself?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi Rita,
First I have flashed the (LF_v5.4.y-1.0.0) demo image in i.MX8M Quad Evk and board boot up successfully.
After that i have create custom layer in yocto and build the custom images.
I have flashed the custom images but system doesn't boot-up. After that I have flashed demo images but board not boot-up.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
For the demo images can work, we have tested on our board. You make sure the boot mode and boot command are right. You can retry it.