i.MX 8MP thermal sensors are swapped

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8MP thermal sensors are swapped

152 Views
martinetd
Contributor IV

Hi

 

This is really minor, but a user asked us about thermal zones on i.MX 8MP and the behavior didn't make sense with what we had documented (adding cpu load makes thermal_zone1 raise faster than zone0, whereas according to the `type` file zone0 ought to be the cpu sensor)

 

Checking the reference manual, it seems to agree that zone0 is ANAMIX vs. zone1 cpu, so the DTS is probably wrong.

 

excerpt from the reference manual:

- The TMU has access to two temperature measurement sites located on the chip. The main probe is located inside of the ANAMIX, while the remote probe is located near the ARM core. The TMU monitors these sites and can signal an alarm if a programmed threshold is ever exceeded. The upper and lower temperature range is continuously captured. A set of reporting registers allow for reading the current temperature at monitored sites.

- also in TMU_TPS bits description we have "00 select the main probe only" // "01 select the remote probe(near A53) only", confirming index 0 = anamix and index1 = cpu (in TRITSR and other registers the description only says probe0 and probe1...)

 

While in dts cpu-thermal uses tmu 0 and soc-thermal uses tmu 1, which is the other way around.

 

The thresholds are identical so this has no impact in practice; this is just a head's up.

0 Kudos
Reply
2 Replies

110 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @martinetd 

 

Thanks for your feedback,  I am checking it and will get it back to you later.

 

Regards

Daniel

17 Views
danielchen
NXP TechSupport
NXP TechSupport

I am confirm this issue with BSP engineer,  and will get it back to you once I have any results.

0 Kudos
Reply