i.MX 8M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,010件の閲覧回数
PMZ6
Contributor I

What development tools do I need to work with the i.MX 8M? To develop for the M4 core? Are there any free IDE tools offered by NXP for this processor? Are there any code/application examples for this processor? Specifically how to assign peripherals to the M4, how to start or run the application on the M4.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,962件の閲覧回数
akbar123
Contributor III

Hi,

As igor said, download SDK. There are some example programs in it.

You can load examples on both DDR and TCM memory, so there are two different build scripts each with release and debug version.

Build one Example for TCM, i.e. run the script without ddr in its name.

To load the program, you can use UBoot or Jtag Programmer.

For UBoot, you can use the below commands:

u-boot=> tftpboot 0x48000000 ${serverip}:<example.bin>
u-boot=> cp.b 0x48000000 0x7e0000 0x20000
u-boot=> bootaux 0x7e0000

Be careful that as the address used in uboot is for TCM, you need to use the script without <ddr> in its name.

Hope it helps you

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,963件の閲覧回数
akbar123
Contributor III

Hi,

As igor said, download SDK. There are some example programs in it.

You can load examples on both DDR and TCM memory, so there are two different build scripts each with release and debug version.

Build one Example for TCM, i.e. run the script without ddr in its name.

To load the program, you can use UBoot or Jtag Programmer.

For UBoot, you can use the below commands:

u-boot=> tftpboot 0x48000000 ${serverip}:<example.bin>
u-boot=> cp.b 0x48000000 0x7e0000 0x20000
u-boot=> bootaux 0x7e0000

Be careful that as the address used in uboot is for TCM, you need to use the script without <ddr> in its name.

Hope it helps you

0 件の賞賛
返信
2,918件の閲覧回数
PMZ6
Contributor I

Having successfully built the SDK examples, how do I invoke the UBOOT command line?

0 件の賞賛
返信
3,000件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Paul

 

one can try mcuxpresso sdk for i.MX8MQ EVK board, available on

https://mcuxpresso.nxp.com/en/welcome

 

Best regards
igor

0 件の賞賛
返信
2,918件の閲覧回数
PMZ6
Contributor I

Thank you Igor, I am able to successfully build M4 examples from the SDK.

0 件の賞賛
返信