Hello
I am trying to get the PPS of the ENET QoS module to work, on an i.MX 8M plus.
And I need some clarification on the differences between the ENET_QOS_1588_EVENTx and the PPSx.
Firstly I thought, that the ENET_QOS_1588_EVENTx is simply the output of the PPSx. However:
When writing 0x02 to the IOMUXC_SW_MUX_CTL_PAD_SAI2_TXFS register (Select ALT2 ENET_QOS_1588_EVENT3), a PPS? is visible at the pin (when PTP is enabled with ptp4l).
But no config of a PPS does anything to it (eg. writing 0x50d7a960 to MAC_HW_FEATURE2 to disable all PPS).
So what is the difference between the ENET_QOS_1588_EVENTx and the PPSx?
Is the ENET_QOS_1588_EVENTx simply the output of the PPSx? If so, Why can I not change anything at the output?
If they are independent functionalities, on what does the event trigger, how can I manipulate it? And which pins can be used as an output of the PPS?
Sadly, I cannot find anything to these questions in the reference manual or the datasheet.
Regards and thanks for your help
解決済! 解決策の投稿を見る。
Thanks for the clarification!
My mistake was, that I thought, that the base address of the enet_qos was at 4043_C000h, as specified in chapter 11.7.6.1.1 "ENET_QOS memory map" of the reference manual. The correct base address is 30BF_0000h as specified in 2.5 "AIPS Memory Maps".
Is there some reason, for the different address in chapter 11.7.6.1.1? Or is this an error in the reference manual?
Regards
Hi @flobue
I hope you are doing well.
One can use the ENET_QOS_1588_EVENTx_OUT pin to output the PPS signal.
PPSOUTNUM[26:24] bit of MAC_HW_FEATURE2 register seems to be a read-only register and it indicates the number of PPS outputs.
It does not disable PPS outputs.
Please refer to 11.7.2.5.8 Flexible Pulse-Per-Second Output in i.MX 8M Plus Applications Processor Reference Manual for more information.
Thanks & Regards,
Sanket Parekh
Thanks for the clarification!
My mistake was, that I thought, that the base address of the enet_qos was at 4043_C000h, as specified in chapter 11.7.6.1.1 "ENET_QOS memory map" of the reference manual. The correct base address is 30BF_0000h as specified in 2.5 "AIPS Memory Maps".
Is there some reason, for the different address in chapter 11.7.6.1.1? Or is this an error in the reference manual?
Regards
Hi @flobue