i.MX 8M Plus Reference Manual

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Plus Reference Manual

6,116 Views
arturpeckerd
Contributor I

Hello,

I would like to know about iMX8M Plus features supported more in detail such as reference manual.

The corresponding documentation link:

Home -> Processors and Microcontrollers -> Arm Processors -> i.MX Applications Processors -> i.MX 8 Processors -> i.MX8M Plus

Does not include a reference manual.

Will be available some day? 

Thanks,

-Carlos 

Labels (1)
4 Replies

6,013 Views
AlejandroV
Contributor I

Hello,

Any update on when will the reference manual it be available on the webpage ? 

Thanks,

Alejandro

0 Kudos
Reply

5,985 Views
AlejandroV
Contributor I

Hey!

Checked again, it just became available at: 

i.MX 8M Plus < Documentation < Reference Manual

5,975 Views
arturpeckerd
Contributor I

Yes, it is great however there are many chapters will be added in a later revision. So now wait for the next seasson to get those or some chapters. 

0 Kudos
Reply

6,102 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Yes, as you may know the i.MX 8MPlus is still in pre-production stage, once it is released the documentation should be available on our webpage.

Best regards,
Aldo.

0 Kudos
Reply