i.MX 8M Plus Cortex-M7 code/data trace into ETF

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M Plus Cortex-M7 code/data trace into ETF

173 次查看
tadejm
Contributor I

Hi all,

I am having some issues in getting ETM/ITM (data/code) trace from Cortex-M7 into ETF/ETR. There is a schema I found in reference manual in attachment.

My notes (please observe also attached image when reading this):

  1. ETM (code) trace works for me from Cortex-A53 core, so it seems that green path is operational.
  2. ETM/ITM (code/data) trace does not work for me from Cortex-M7 core, so it seems orange path is not operational
  3. As you can see in image there are 3 ATB Funnels (marked with numbers)

My questions:

  1. There are 3 ATB Funnels, but in debug memory map I only found 2:
    1. On APB bus (APSEL 1) on address 0x80C03000 <- I assume this is either funnel #1 or #2 on image above (this one is also documented in Reference Manual)
    2. On AHB (M7) bus (APSEL 4) on address 0xE0043000 <- I assume this is funnel #3 on image above (this one is not documented in Reference Manual)
    3. Where is the third one?
  2. Is there something else that should be configured for Cortex-M7 core trace to work?

Thank you for your help.

0 项奖励
回复
0 回复数