i.MX 8M Plus Applications Processor Reference Manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 8M Plus Applications Processor Reference Manual

ソリューションへジャンプ
5,147件の閲覧回数
marcelziswiler
Senior Contributor I

Thank you very much for publishing an initial reference manual. I was very excited in high hopes to find badly needed answers to some questions but quickly faced reality meaning most chapters are completely missing resp. there is only a placeholder! Could you please explain the overall strategy behind this? When exactly may we expect a complete reference manual being published? Thanks!

0 件の賞賛
返信
1 解決策
5,113件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Unfortunately these chapter will be added in next revision. You can open a case and see if you can obtain the compete reference manual.

 

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,133件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello marcelziswiler,

The reference manual is in the webpage is the latest release, if you have one of chapter are bad please clarify your query, in order to fix it.

 

Regards

 

0 件の賞賛
返信
5,122件の閲覧回数
marcelziswiler
Senior Contributor I

OK, well, did you actually bother having a look at the published one? Anyway, please find the list of missing information below and let me know if you have any further doubts about what exactly I am talking about. Just to make sure you did not miss my initial questions, let me reiterate them here again as well: Could you please explain the overall strategy behind this? When exactly may we expect a complete reference manual being published? Thanks!

Chapter 5
Arm Cortex A53 Platform (A53) Placeholder

Chapter 7
Messaging Unit (MU) Placeholder

Chapter 10
Network Interconnect Bus System (NIC) Placeholder

Chapter 12
Shared Peripheral Bus Arbiter (SPBA) Placeholder

Chapter 13
TrustZone Address Space Controller (TZASC) Placeholder

Chapter 15
System JTAG Controller (SJC) Placeholder

Chapter 16
System Counter (SYS_CTR) Placeholder

Chapter 17
Clock Control Module (CCM) Placeholder

Chapter 19
Crystal Oscillator (XTALOSC) Placeholder

Chapter 20
Thermal Monitoring Unit (TMU) Placeholder

Chapter 23
On-Chip OTP Controller (OCOTP_CTRL) Placeholder

Chapter 25
System Reset Controller (SRC) Placeholder

Chapter 26
Watchdog Timer (WDOG) Placeholder

Chapter 30
Interrupt Request Steering (IRQ_STEER) Placeholder

Chapter 32
IOMUX Controller (IOMUXC) Placeholder

Chapter 34
External Memory Overview Placeholder

Chapter 35
DDR Controller (DDRC) Placeholder

Chapter 36
DDR BLK_CTRL Placeholder

Chapter 37
DDR PHY (DDR_PHY) Placeholder

Chapter 38
AHB-to-APBH Bridge with DMA (APBH-Bridge-DMA) Placeholder

Chapter 39
62BIT Correcting ECC Accelerator (BCH) Placeholder

Chapter 40
General Purpose Media Interface (GPMI) Placeholder

Chapter 41
Enhanced Configurable SPI (ECSPI) Placeholder

Chapter 42
FlexSPI Controller (FlexSPI) Placeholder

Chapter 44
HSIO BLK_CTRL Placeholder

Chapter 45
Universal Serial Bus Controller (USB) Placeholder

Chapter 46
Universal Serial Bus PHY (USB_PHY) Placeholder

Chapter 47
PCI Express (PCIe) Placeholder

Chapter 48
PCI Express PHY (PCIe_PHY) Placeholder

Chapter 49
Ethernet MAC (ENET) Placeholder

Chapter 50
Ethernet Quality Of Service (ENET_QOS) Placeholder

Chapter 55
MEDIA BLK_CTRL Placeholder

Chapter 57
Image Sensing Interface (ISI) Placeholder

Chapter 58
MIPI CSI Host Controller (MIPI_CSI) Placeholder

Chapter 59
MIPI DSI Host Controller (MIPI_DSI) Placeholder

Chapter 60
MIPI D-PHY (MIPI_DPHY) Placeholder

Chapter 61
LVDS Display Bridge (LDB) Placeholder

Chapter 62
HDMI TX Controller Placeholder

Chapter 63
HDMI TX PHY Placeholder

Chapter 64
HDMI TRNG Controller Placeholder

Chapter 65
HDMI TX BLK_CTRL Placeholder

Chapter 66
HDMI TX Parallel Audio Interface (HTX_PAI) Placeholder

Chapter 67
HDMI TX Parallel Video Interface (HTX_PVI) Placeholder

Chapter 68
Image Signal Processor (ISP) Placeholder

Chapter 69
DeWarp Placeholder

Chapter 70
Machine Learning Neural Processing Unit (NPU) Placeholder

Chapter 72
AUDIO BLK_CTRL Placeholder

Chapter 73
PDM Microphone Interface (MICFIL) Placeholder

Chapter 74
Synchronous Audio Interface (SAI) Placeholder

Chapter 75
Asynchronous Sample Rate Converter (ASRC) Placeholder

Chapter 76
Enhanced Audio Return Channel (eARC) Placeholder

Chapter 77
Audio DSP (HiFi 4 DSP) Placeholder

Chapter 79
2D Graphics Processing Unit (GPU2D) Placeholder

Chapter 80
3D Graphics Processing Unit (GPU3D) Placeholder

Chapter 81
VPU G1 Decoder Placeholder

Chapter 82
VPU G2 Decoder Placeholder

Chapter 83
VPU VC8000E Encoder Placeholder

Chapter 84
VPU BLK_CTRL Placeholder

Chapter 85
I2C Controller (I2C) Placeholder

Chapter 86
Universal Asynchronous Receiver/Transmitter (UART) Placeholder

5,114件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Unfortunately these chapter will be added in next revision. You can open a case and see if you can obtain the compete reference manual.

 

Regards

0 件の賞賛
返信