uSDHC shared resources

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uSDHC shared resources

2,254 次查看
RooperK
Contributor I

I have encountered a bit of understanding gap in which parts of a controller are common and which are dedicated to each channel.

  1. Do reset registers on SYS_CTRL(RSTC, RSTD and RSTA) reset whole circuit or only channel, on which they are set(also, are RSTC and D necessary before RSTA)?
  2. Are DLL and clock seperate or each time driver operates with another card it has to switch clock?
标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

2,243 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rooper

 

1. for uSDHC usage one can look at SDK example

https://github.com/RT-Thread/rt-thread/tree/master/bsp/imx6sx/iMX6_Platform_SDK/sdk/drivers/usdhc

2. all uSDHC instances are independent modules. So SYS_CTRL resets only one module.

 

Best regards
igor

0 项奖励
回复

2,238 次查看
RooperK
Contributor I

Thank you for answer. As I understand, since each instance is seperate module, buffer, DLL and clock are seperate too? Documentation specifies broadcast commands, which are send to all cards. Are they confined to module or send to all modules?

0 项奖励
回复

2,227 次查看
igorpadykov
NXP Employee
NXP Employee

yes they are separate.

 

Best regards
igor

0 项奖励
回复