i.MX 8M Mini QuadLite. Floating Point Unit (FPU) Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Mini QuadLite. Floating Point Unit (FPU) Support

Jump to solution
3,371 Views
mklnc
Contributor I

Hi,

We're using MIMX8MM5CVTKZAA, i.MX 8M Mini QuadLite processor with quad core Arm Cortex-A53.  There is FPU support on the Arm Cortex-A53 MPCore™ Platform side, right? 

While FPU support in Quad Core A53 CPU is mentioned in the i.MX 8M Mini Applications Processor Datasheet document, FPU support is mostly mentioned in M4 CPU in the i.MX 8M Mini Applications Processor Reference Manual document.

Could you please check chapter 4 of the i.MX 8M Mini Applications Processor Reference Manual?

Thnx,

Merve

Labels (1)
0 Kudos
Reply
1 Solution
3,351 Views
b36401
NXP Employee
NXP Employee

A53 cores in i.MX8M series have FPU.
Please note that you need to pass "-mfloat-abi=hard -mfpu=fpv4-d16" to the compiler to compile code using FPU features of the core.

View solution in original post

1 Reply
3,352 Views
b36401
NXP Employee
NXP Employee

A53 cores in i.MX8M series have FPU.
Please note that you need to pass "-mfloat-abi=hard -mfpu=fpv4-d16" to the compiler to compile code using FPU features of the core.