i.MX 8M Family DDR Register Programming Aid (RPA)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Family DDR Register Programming Aid (RPA)

3,249 Views
norton
Contributor II

I'm having an issue creating a DDR stress test file for 2GB LPDDR4.

The Register Configuration generates a stress test file that is the same as a 4GB LPPDDR4 file.

Please compare the files I have included and advice.

Labels (1)
0 Kudos
Reply
2 Replies

3,158 Views
norton
Contributor II

I figured out my problem. I had the "Number of Chip Selects used" wrong.

I had the number of chip selects as 2 in stead of 1. 

I was thinking total number of chip selects not chip selects per channel.

Thanks for your help.

3,158 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Michael Norton,

I was reviewing other stress tool scripts and it’s my understanding that the RAM size is detected by the stress test tool. It can additionally be selected from the GUI. If both memories have similar timing parameters and number of addresses row and columns the scrips could be identical. Have you tested this script on both kinds of boards?

I hope this helps!
Regards,

0 Kudos
Reply