i.MX 8M Development kit for AVS Set-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8M Development kit for AVS Set-up

3,095 Views
shibani
Contributor I

Hi,

I am working on the i.MX 8M Devlopement kit for AVS on the PICO-PI-IMX8M TechNexion Online Store TechNexion and NXP Development Kit for Amazon Alexa Voice Service .

I am having trouble locating the AVS SDK files  that are supposed to be there on the root directory. I have attached the image of the putty terminal, there seem to be no files in the home/root folder. I was under the impression the AVS sdk would be available, am I missing something?

Labels (1)
0 Kudos
Reply
3 Replies

2,814 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please send me the steps of how you initialized and built the avs image?

Best Regards,

Diego

0 Kudos
Reply

2,814 Views
shibani
Contributor I

Hello Diego,

I was following the instructions provided in the User Guide for IMX8M devlopment kit for avs guide provided by NXP. Would the folllowing link: Alexa SDK support for NXP i.MX Boards  work on the PICO-PI IMX8m AVS devlopment board?

Thank you,

Shibani Abhyankar

0 Kudos
Reply

2,814 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

At the time you are building the image when is asking you about pre-installing the AVS SDK software, are you writing that yes or no?

Best Regards,

Diego.

0 Kudos
Reply