i.MX 8 Mini cannot boot from Linux and not able to switch to Android

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8 Mini cannot boot from Linux and not able to switch to Android

跳至解决方案
6,833 次查看
littlebone
Contributor II

Hi all,

I flashed my i.MX8 Mini with the Linux image (L5.4.70_2.3.0_images_MX8MMEVK.zip) I downloaded from the official website and it worked well.

And then I tried to switch back to android image (android_p9.0.0_1.0.0-ga_image_8mmevk) also downloaded from the official website. But uuu is always blocked and keep repeating the "write -f u-boot-imx8mm-evk-uuu.imx -offset 0x57c00" step.

Since it does not work, I switched it back to Linux image again with the same image above. Though I can successfully flash the image, the board does not boot and looks like it is keeping reset again and again (The green D1 cpu and red D708 power LED goes off for a short instant every a few second).

Hopefully I could find some help here. Thank you.

标签 (2)
0 项奖励
回复
1 解答
6,807 次查看
littlebone
Contributor II

Confirmed that the problem was caused by one wrong on/off setting on the switch. Thank you. 

在原帖中查看解决方案

5 回复数
6,808 次查看
littlebone
Contributor II

Confirmed that the problem was caused by one wrong on/off setting on the switch. Thank you. 

6,790 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Good news it works.

0 项奖励
回复
6,821 次查看
littlebone
Contributor II

BTW I am flashing the image with the instructions I found on NXP website (uuu.exe L4.14.78_1.0.0_ga_images_MX8MMEVK.zip and uuu.exe uuu-android-mx8mm-evk-sd.lst)

0 项奖励
回复
6,821 次查看
littlebone
Contributor II

Hi b45499,

Correct me if I am wrong, as I know the switch setting is the same for Android/Linux BSP before flashing/after flashed. That is, set to SDP mode before flashing and switch set to boot from eMMC mode after flashed. Thank you.

0 项奖励
回复
6,821 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Have you set the right boot mode for your board to boot up? For linux and android download and boot up you can see our user guide, details in our documents.

 

0 项奖励
回复