i.MX 7Dual Ethernet Throughput Performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 7Dual Ethernet Throughput Performance

2,320 次查看
tonywk
Contributor I

Hi team,

Could you provide the report of 1G Ethernet Throughput Performance of i.mx 7?

The processor is MCIMX7D7DVM10SD.

 

Thanks.

0 项奖励
回复
6 回复数

1,609 次查看
tonywk
Contributor I

Hi NXP team,

I test Ethernet bi-direction throughput speed of MCIMX7D-SABRE Rev C EVB.

ENENT1 is bridged with ENENT2, the bi-direction throughput speed is around 767Mbps.

MCIMX7D-SABRE_Ethernet_bridge_throughput.png

And the throughput test result in my product is around 923Mbps.

image017.png

Can you help to confirm the Ethernet  throughput result is acceptable in both EVB and my product?

Thanks.

0 项奖励
回复

2,243 次查看
tonywk
Contributor I

Hi @joanxie ,

Is it possible to have the result of RX/TX bidirection throughput?

Thanks.

0 项奖励
回复

2,228 次查看
joanxie
NXP TechSupport
NXP TechSupport

I didn't find such report intnernally

0 项奖励
回复

2,303 次查看
joanxie
NXP TechSupport
NXP TechSupport

this is performance for imx6sx, but imx7d can refer to this too

"Ethernet benchmark figures, CPU at 1GHz, TX:870Mbps, RX:930Mbps"

0 项奖励
回复

2,289 次查看
tonywk
Contributor I

Hi @joanxie ,

Thanks for the prompt reply.

"Ethernet benchmark figures, CPU at 1GHz, TX:870Mbps, RX:930Mbps"

Is the result that test both the Ethernet TX and RX throughput in the same time?

 

Thanks.

0 项奖励
回复

2,275 次查看
joanxie
NXP TechSupport
NXP TechSupport

 should test RX and TX separately, I don't find RX/TX bidirection result

0 项奖励
回复