i.MX 7Dual Ethernet Throughput Performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 7Dual Ethernet Throughput Performance

2,319件の閲覧回数
tonywk
Contributor I

Hi team,

Could you provide the report of 1G Ethernet Throughput Performance of i.mx 7?

The processor is MCIMX7D7DVM10SD.

 

Thanks.

0 件の賞賛
返信
6 返答(返信)

1,608件の閲覧回数
tonywk
Contributor I

Hi NXP team,

I test Ethernet bi-direction throughput speed of MCIMX7D-SABRE Rev C EVB.

ENENT1 is bridged with ENENT2, the bi-direction throughput speed is around 767Mbps.

MCIMX7D-SABRE_Ethernet_bridge_throughput.png

And the throughput test result in my product is around 923Mbps.

image017.png

Can you help to confirm the Ethernet  throughput result is acceptable in both EVB and my product?

Thanks.

0 件の賞賛
返信

2,242件の閲覧回数
tonywk
Contributor I

Hi @joanxie ,

Is it possible to have the result of RX/TX bidirection throughput?

Thanks.

0 件の賞賛
返信

2,227件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I didn't find such report intnernally

0 件の賞賛
返信

2,302件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

this is performance for imx6sx, but imx7d can refer to this too

"Ethernet benchmark figures, CPU at 1GHz, TX:870Mbps, RX:930Mbps"

0 件の賞賛
返信

2,288件の閲覧回数
tonywk
Contributor I

Hi @joanxie ,

Thanks for the prompt reply.

"Ethernet benchmark figures, CPU at 1GHz, TX:870Mbps, RX:930Mbps"

Is the result that test both the Ethernet TX and RX throughput in the same time?

 

Thanks.

0 件の賞賛
返信

2,274件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

 should test RX and TX separately, I don't find RX/TX bidirection result

0 件の賞賛
返信