i.MX 6UltraLite Hardware design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6UltraLite Hardware design

1,242 Views
ricardoferreira
Contributor II

Hi,


In the schematic of the i.MX 6UltraLite there is a component UM805RE that should be an Votlage monitor 2.63V with 4 pins. I can't find it in any of the usual suppliers.

Can anyone suggest any good alternative to this component?

Tags (1)
2 Replies

1,043 Views
almarto
Contributor IV

You could also use tc1270arvrctr from Microchip

BR

1,043 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ricardo

probably one can look at ADM671_R (ADM6711) from analog devices.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------