i.MX 6SoloLite - Camera function supportability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6SoloLite - Camera function supportability

2,207件の閲覧回数
balajykumar
Contributor I

Hi

I am using IMX6SoloLite Processor in my Design. i just want to comfirm that whethere this processor will support camera interface? Because i am planning to add Camera device in my application. Can anyone help in this?

Thanks

Balajy

0 件の賞賛
返信
3 返答(返信)

2,102件の閲覧回数
pankajrana
Contributor III

Hi Balajy,

Yes, i.Mx6 SoloLite does support camera interface. It has got Parallel Camera port, mentioned in the processor documentation.

~Pankaj Rana

0 件の賞賛
返信

2,102件の閲覧回数
balajykumar
Contributor I

Hi

Thanks for the reply. I just want the information of how much resolution and mega pixel Or(fpi) of camera device it can support. Is it required any software block should enable in the processor?

Please clarify.

Thanks

Balajy

0 件の賞賛
返信

2,102件の閲覧回数
art
NXP Employee
NXP Employee

The parallel Camera Sensor Interface (CSI) module of the i.MX6SoloLite processor can provide up to 16-bit wide data port (mostly for Raw data) and up to 66MHz pixel clock. For details, please refer to the Chapter 16 of the i.MX6SoloLite Reference Manual Rev.2 document, available on the Freescale web site:

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信