i.MX 6 USB device-mode driver for FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6 USB device-mode driver for FreeRTOS

ソリューションへジャンプ
1,934件の閲覧回数
normcampbell
Contributor I

I'm considering using an i.MX 6 UltraLite in a small realtime system and USB device mode is a requirement. I'd like to use FreeRTOS rather than Linux (because of the realtime requirement) but I can't find a USB device driver for it. Is there a FreeRTOS driver for a similar ARM part that I could adapt, or could I adapt the linux USB driver for use with FreeRTOS? Other suggestions? Thx.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,750件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Norm Campell,

About the BSP released in our website for i.MX6UL is linux BSP.  We recommend customers to use the released BSP in our website. About the FreeRTOS is out of our support, so sorry, you have to modify and do porting yourself.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,751件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Norm Campell,

About the BSP released in our website for i.MX6UL is linux BSP.  We recommend customers to use the released BSP in our website. About the FreeRTOS is out of our support, so sorry, you have to modify and do porting yourself.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct  button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信