i.MX 6 QP Select Input Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 6 QP Select Input Register

1,284 Views
TaikiSugiura
Contributor I

Hi, 

I design register settings for i.MX6QP.

Is it necessary to set Select Input Register only when one function is set to multiple Pads in Pad Mux Register?

Or is it always necessary to set Select Input Register even when one function is set to one Pad?

Labels (1)
0 Kudos
Reply
1 Reply

1,274 Views
igorpadykov
NXP Employee
NXP Employee

Hi Taiki

 

>is it always necessary to set Select Input Register even when one function is set to one Pad?

 

this depends on particular pad/function so necessary to check Chapter 36  IOMUX Controller (IOMUXC)

i.MX 6DualPlus/6QuadPlus Applications Processor Reference Manual

as in example below, ALT1 requires it, ALT0 - not :

 

1.jpg

 

Best regards
igor

0 Kudos
Reply