Issues while porting the MIPI DSI panel driver to Uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues while porting the MIPI DSI panel driver to Uboot

1,033 Views
sd05
Contributor III
Hi NXP Community Members,
We are facing issues while porting the MIPI DSI panel driver to Uboot.
We have our customized ST7703 panel, which we have successfully ported at the kernel layer with VAR-DART-MX8MM and the same is working fine. As we want to enable the splash screen, we tried to port the same driver at the u-boot layer, based on the rm67191 reference panel driver.
Our LCD is connected directly to the MIPI DSI interface. Post porting, we are able to see that the probe and initialization of panel are going correct, logs as attached. But the MIPI clock and LCDIF clock registers are not getting set.
We strongly feel that there is some issue with the clock settings at the u-boot level. Following are the differences in the register values at the kernel and u-boot levels.
 
 
RegisterRegister addrKernel LayerUboot Layer
LCDIF_CTRL10x100x30721000x70100
LCDIF_CUR_BUF0x400x0 to 0x781000000xbf000000
LCDIF_NEXT_BUF0x500x781000000xbf000000
LCDIF_VDCTRL00x700x103000030x11300003
 
 
As mentioned above these are the value dumps between the kernel layer and u-boot layer. And as communicated on the portal, without changing these registers variscite is able to use the RM67191 panel, then why do we need to change these register settings. We have tried your following commit id:
 
And we are using the u-boot version: imx_v2020.04_5.4.24_2.1.0_var02
 
We request your help on the same.
Thanks in advance!
0 Kudos
Reply
0 Replies