Hi.
In i.MX 6 BSP Porting Guide 1.2.1 Preparing the Code
I created a script, as suggested:
#!/bin/bash
export ARCH=arm
export CROSS_COMPILE=/opt/poky/1.7.1/sysroots/x86_64-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi-
make distclean;
make mx6vega_config
make
but when the script error occurs - /cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi-gcc: No such file or directory
Indeed, in my folder I can not find /cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi-
已解决! 转到解答。
Hi. I solved the problem. I installed meta-toolchain https://community.freescale.com/docs/DOC-94849.
Сhanged in the script path, and after that I was compiled U-Boot.:smileyhappy:
but when the script error occurs - /cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi-gcc: No such file or directory
Did you notice the '/' in front of the path? I assume that this is why you see the error.
Indeed, in my folder I can not find /cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi-
This sentence answers the question on your own. Whe you can't find the path to the compiler direction, how should the shell find it.
Make sure you hav installed the arm-poky-linux compiler into some folder (eg. /opt/poky/...), add the path to your bin directory, located into the compiler folder, to your PATH environment variable (export PATH=/opt/poky/...:$PATH) and let the CROSS_COMPILE variable point to the same place, including 'arm-poky-linux-gnueabi-' which is a prefix for the compiler you are using to compile the kernel or whatever.
Hello.
Thank you for your posts!
I'm trying to compile the Linux for custom board.
To do this, I follow recommendations "i.MX 6 BSP Porting Guide"
"Make sure you hav installed the arm-poky-linux compiler into some folder (eg. / Opt / poky / ...),"
How do I install it? I am new to Linux, so I refer to "Freescale_Yocto_Project_User's_Guide."
In Yocto Training - https://community.freescale.com/docs/DOC-94849, proposed to install "meta-toolchain"
It's something that I need to install?
Hi. I solved the problem. I installed meta-toolchain https://community.freescale.com/docs/DOC-94849.
Сhanged in the script path, and after that I was compiled U-Boot.:smileyhappy:
export CROSS_COMPILE=/opt/poky/1.7.1/sysroots/x86_64-pokysdk-linux/usr/bin/cortexa9hf-vfp-neon-poky-linuxgnueabi/arm-poky-linux-gnueabi- Instead of this .
Is the below path is available?
export CROSS_COMPILE=/opt/poky/1.7.1/sysroots/x86_64-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-
No. In folder "opt/poky/1.7.1/sysroots/x86_64-pokysdk-linux/usr/bin" there are no directories.
In this folder i install "Pre-Built buildtools
Tarball"(Yocto Project Reference Manual).
Hello Eugene,
What do you trying to build (application, drivers)? Are you using Freescale dev board and which flavour of kernel and distribution you are using?
Second, you need a cross-compiler toolchain with gcc, libraries, headers to build for imx6. You can download it as Freescale suggested or from linaro website. They have references for Cortex-A9 which is imx6
export path to your toolchain binaries, for example: export PATH=$PATH:/usr/local/toolchain/arm-linux-gnueabi/bin
In any case, describe in more details what are you planning to build.
Regards,
Konstantyn Prokopenko.