http://bitshrine.org/gpp not available

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

http://bitshrine.org/gpp not available

ソリューションへジャンプ
2,249件の閲覧回数
BrilliantovKiri
Senior Contributor I

Hello!

I start work with imx287 CPU, for this I download L2.6.35_1.1.0_130130_source.tar.gz from FreeScale site and install it.

.config

CONFIG_CONFIG_TITLE="GNU/Linux Target Image Builder : Platform Selection"

CONFIG_PLATFORM_imx=y

CONFIG_PLATFORM_DIR="config/platform/imx"

config/platform/imx/.config

CONFIG_CONFIG_TITLE="Freescale iMX28 Based Boards"

CONFIG_PLATFORM_COMMENT="Freescale iMX28 Based Boards"

CONFIG_VENDOR="Freescale"

CONFIG_PLATFORM="imx28"

CONFIG_PLATFORM_SUBDIR="imx"

CONFIG_GNUTARCH="arm"

CONFIG_LINTARCH="arm"

CONFIG_CFGHOST="arm-linux"

CONFIG_ARMEABI_ARCH=y

# CONFIG_VFP_ARCH is not set

..........

#

# Toolchain selection.

#

CONFIG_TOOLCHAIN_ARMEABI_FSL_GCC_LINARO_MULTILIB=y

# CONFIG_TOOLCHAIN_ARMEABI_FSL_GCC_MULTILIB is not set

# CONFIG_TOOLCHAIN_ARMEABI_CODE_SOURCERY is not set

# CONFIG_TOOLCHAIN_ARMEABI_GLIBC1 is not set

# CONFIG_TOOLCHAIN_ARMEABI_CUSTOM is not set

CONFIG_TOOLCHAIN="gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm"

CONFIG_TOOLCHAIN_PATH="/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain"

CONFIG_TOOLCHAIN_PREFIX="arm-none-linux-gnueabi-"

CONFIG_TOOLCHAIN_CFLAGS=""

When I try install gcc LTIB exit with error:

$ ./ltib

Installing: gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm

Testing network connectivity

OK GPP:

Try gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm.md5 from the GPP

http://bitshrine.org/gpp/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm.md5:

09:48:40 ERROR 404: Not Found.

Try gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm from the GPP

http://bitshrine.org/gpp/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm

:

09:48:40 ERROR 404: Not Found.

Can't get: gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm at ./ltib line 2560.

Died at ./ltib line 2560.

traceback:

main::check_toolchain_setup:2560

  main::pre_build_checks:1465

   main:569

I try look http://bitshrine.org/gpp directrory from browser, but I see only not authed messsage.

How can I solve this problem?

Thank you and excuse my bad english.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,219件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please check if gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm (and its .md5) is present
in /opt/freescale/pkgs.

If - not, please place it there.
The gcc-4.6.2 may be found in pkgs directory of i.MX6 packages  in xxx_source.tar.gz\ xxx_source\pkgs\

directory. 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

Also, you may look at the next thread :
 

“Can't get: gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm at ./ltib line 2560.”


https://community.freescale.com/thread/304744


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,220件の閲覧回数
Yuri
NXP Employee
NXP Employee

  Please check if gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm (and its .md5) is present
in /opt/freescale/pkgs.

If - not, please place it there.
The gcc-4.6.2 may be found in pkgs directory of i.MX6 packages  in xxx_source.tar.gz\ xxx_source\pkgs\

directory. 

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

Also, you may look at the next thread :
 

“Can't get: gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12-1.i386.rpm at ./ltib line 2560.”


https://community.freescale.com/thread/304744


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信