how to16c554 Using the imx6dl eim

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to16c554 Using the imx6dl eim

2,860件の閲覧回数
tommykim
Contributor I

Now I use imx6dl     LTIB   ,   L3.0.35  

I connected 16c554 to  eim port(use 8bit data,Non mux)

how to set board config ????

plz help.... 

0 件の賞賛
返信
2 返答(返信)

2,673件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi tommykim

one can check 16c55x driver which is present in i.MX31PDK 1.5 Linux BSP (i.MX31 has similar weim module)
http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/arm-mcus-and-mpus/i....

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,673件の閲覧回数
tommykim
Contributor I

Hi igorpadykov 

first of all 

Thanks 

But I can't find configuration......

where is it???? 

Please help..

0 件の賞賛
返信