how to use watchdog in imx8 m40 without modifing scfw

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use watchdog in imx8 m40 without modifing scfw

1,372件の閲覧回数
974782852
Contributor II

My project will use the watchdog in imx8 m40/

In code i test a situation---trigger the watchdog, but the whole system hangs on include linux of A core。

By reading the scfw_port.pdf, there is a way to use watchdog correctly that is to modify the scfw to create the partition for m40 watchdog.

But the scfw operation is dangerous, so afraid to

0 件の賞賛
返信
1 返信

1,314件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eric

I am afraid it is not possible as all resource management is handled by SCU using

SCFW APIs. On link below there is example for moving FlexCAN resources to  A cores partition:

System Controller Firmware 101 - Resource management service 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信