how to use to implement overlay in hardware imx6dl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use to implement overlay in hardware imx6dl

11,253 Views
wangds
Contributor I

Now I used imx6Dual. Fb0 is available at present, and FB1 is not specified. At present, it is hoped to implement overlay on the screen. A bottom layer is used to display the video stream information from camera through device node , and an upper layer displays the normal interface in QT.What should I do?

Tags (2)
0 Kudos
Reply
1 Reply

1,014 Views
igorpadykov
NXP Employee
NXP Employee

Hi wang

please look at suggestions on

How to implement qt/embedded + gstreamer in imx6 with alpha function? 

Configuring i.MX6 boards for different screens - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply