how to use the I2C_INT in imx28_evk?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use the I2C_INT in imx28_evk?

1,479件の閲覧回数
meifang
Contributor I

In imx28_EVK sch file,the touch screen use a interrupt of the pin I2C_INT.

I can't understand how to work of it. There is no input signal by this pin.

0 件の賞賛
返信
3 返答(返信)

1,385件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang

this signal is not used, it is for optional

LCD touch controller. You can check LCD schematic,

SPF-26139_revB.pdf, JP2 - DNP

MX28_LCD_DESIGN_FILES : i.MX28 LCD Design Files

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,385件の閲覧回数
meifang
Contributor I

Hi chip

thanks very much for your answer so quickly.

If this pin is optional for LCD touch control,how control the interrupt of touch screen?

I used L2.6.35_1.1.0 and tslib-1.0,but the touch not work right.

0 件の賞賛
返信

1,385件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fang

in L2.6.35_1.1.0 pin I2C_INT is not used.

Best regards

chip

0 件の賞賛
返信