how to use ECSPI5 Mater for Externel Device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use ECSPI5 Mater for Externel Device

1,098 Views
JackOh
Contributor I

Hi.

i  am using  SABRE Platform for smart Devices with I.MX6Q

i've already set spidev4.0 for ECSPI5 like a following code .

but i could not  see the signal for SS0,CLK ..etc  . Here is my code , what am i doing wrong ?

1. i added in board-mx6q_sabresd.c

    MX6Q_PAD_SD2_CLK__ECSPI5_SCLK,

    MX6Q_PAD_SD2_CMD__ECSPI5_MOSI,

    MX6Q_PAD_SD2_DAT0__ECSPI5_MISO,

    MX6Q_PAD_SD2_DAT1__ECSPI5_SS0,

2.  i modified iomux-mx6q.h

     MUX_PAD_CTRL( NO_PAD_CTRL)  -> MUX_PAD_CTRL(MX6Q_ECSPI_PAD_CTRL) for all PAD above

3,  finally , i changed board-mx6q_sabread.c as a following code

#define SABRESD_ECSPI5_CS0    IMX_GPIO_NR(1, 14)

static int mx6q_sabresd_spi5_cs0[] = {

    SABRESD_ECSPI5_CS0,

};

static const struct spi_imx_master mx6q_sabresd_spi5_data0 __initconst = {

    .chipselect     = mx6q_sabresd_spi5_cs0,

    .num_chipselect = ARRAY_SIZE(mx6q_sabresd_spi5_cs0),

};

static struct spi_board_info imx6_sabresd_spi_nor_device[] __initdata = {

#if 1

    {

        .modalias = "spidev",

        .max_speed_hz = 20000000, /* max spi clock (SCK) speed in HZ */

        .bus_num = 4,

        .chip_select = 0,

        .mode = SPI_MODE_0,

        .platform_data = NULL,

    },

#endif

};"

imx6q_add_ecspi(4, &mx6q_sabresd_spi5_data0);

spi_device_init();

 

4.  after i rebuild kernel , i can see /dev/spidev4.0 and it was operated succesfully With IOCTL as a spidev_test.c

i added following code in jni for android

static void transfer(int fd)

{

    int ret;

    uint8_t tx[] = {

       0xa5, 0xa5,

    };

    uint8_t rx[ARRAY_SIZE(tx)] = {0, };

    struct spi_ioc_transfer tr = {

        .tx_buf = (unsigned long)tx,

        .rx_buf = (unsigned long)rx,

        .len = ARRAY_SIZE(tx),

        .delay_usecs = 0,

        .speed_hz = 6000000,

        .bits_per_word = 8,

    };

     ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);

    if (ret < 1)

        pabort("can't send spi message");

    for (ret = 0; ret < ARRAY_SIZE(tx); ret++) {

        if (!(ret % 6))

            puts("");

        printf("%.2X ", rx[ret]);

    }

    puts("");

}

mode = SPI_MODE_0;

bits = 8;

speed = 6000000;

fd = open("dev/spidev4.0", O_RDWR);

ret = ioctl(fd, SPI_IOC_WR_MODE, &mode);

ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits);

ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);

transfer(fd);

and i can see return value "2" of ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr) sucessfully

but i could not see the signal for SSO , CLK, etc with Scope

     SS0 -> SD2_DAT1 ( PIN NO #08)

     CLK -> SD2_CLK   (PIN NO #05)

     .etc

 

please help me.

thank you in advance

Labels (2)
0 Kudos
Reply
1 Reply

796 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Let me see if I understand correctly. You were able to make it work using spidev_test.c with the above modifications but it does not work using jni correct?

I wonder if you are able to dump the value of the registers including the IOMUX values. That will help to identify the problem.

Best Regards,

Alejandro

0 Kudos
Reply