Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Rayson,
The answer from Saurabh is also useful.
Have a nice day
Best Regards
Dan
 
					
				
		
 Rita_Wang
		
			Rita_Wang
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Rayson,
You also have to modify the BSP after you have completed configuring the LCD Parameter refer to the LCD datasheet.
Here you can refer to this thread:
LCD not working on custom i.mx6q board
There are details in how to modify, you can have a refer to.
Besides, here I attach you two documents, they are useful for you.
Have a great day
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Dan Wang:
Thanks a lot , but I use the LVDS interface, and the display device is HanntStart HSD101PFW2, and how to set these parameters as follows, I had search the HSD101PFW2's datasheet ,but did not find these paramters , can you help me again , thanks very much。
struct fb_videomode {
const char *name; /* optional */
u32 refresh; /* optional */
u32 xres;
u32 yres;
u32 pixclock;
u32 left_margin;
u32 right_margin;
u32 upper_margin;
u32 lower_margin;
u32 hsync_len;
u32 vsync_len;
u32 sync;
u32 vmode;
u32 flag;
};
 
					
				
		
Hi Rayson
You need to contact local supplier for datasheet.
It you still can't find it than you should try standard WSVGA parameter. It should work.
Thanks
Saurabh
Hi Saurabh:
Thank you very much, where can I get the standard WSVGA paramters,can you help me, thank you again.
 
					
				
		
Hi
Rayson
You can try this.
static struct fb_videomode video_modes[] = {
...
{
.name = "WSVGA",
.refresh = 60,
.xres = 1024,
.yres = 600,
.pixclock = 48000,
.left_margin = 104,
.right_margin = 43,
.upper_margin = 24,
.lower_margin = 20,
.hsync_len = 5,
.vsync_len = 5,
.sync = 0,
.vmode = FB_VMODE_NONINTERLACED,
.flag = 0,
},
Hi Saurabh:
I try it ,but it doesn't work。