how to set our custom board settings in DDR config tool.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to set our custom board settings in DDR config tool.

1,373件の閲覧回数
arka
Contributor III

Hi,

I am trying to create lpddr4x_timing.c for our custom board , to add two FSP support . please help us to create a lpddr4x_timing.c file for our custom board , and how to use DDR config tool to create lpddr4x_config.c file to add custom board settings on DDR config tool?

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,346件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This can be done through DDR tool in Config Tools for i.MX. You need to enter your memory features and this will generate a initialization/timing script for DDR configuration. If you need to change some register value, you can do it in this generated scripts.

Config Tools for i.MX Applications Processors | NXP Semiconductors

Here you can consult more information about how to use the tool:

User Guide for Config tools for i.MX

And here how to implement it in software in section 4.5 Building u-boot image:

MScale DDR tool

Best regards.

0 件の賞賛
返信

1,341件の閲覧回数
arka
Contributor III

Hi jorge,

We need to use User Guide for Config Tools for i.MX
this link document to create lpddr4x_timing.c file , in which section we need to refer,

We have our custom board yocto build, we need to add FSP support on lpddr4x_timing.c file, adding two FSP support on IMX93.

 

タグ(1)
0 件の賞賛
返信

1,324件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please refer to section 6 DDR Tool.

With FSP are you referring to frequency set point?

Best regards.

0 件の賞賛
返信

1,371件の閲覧回数
arka
Contributor III

We have using IMX93 custom board.

タグ(1)
0 件の賞賛
返信