how to set our custom board settings in DDR config tool.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to set our custom board settings in DDR config tool.

1,106 Views
arka
Contributor III

Hi,

I am trying to create lpddr4x_timing.c for our custom board , to add two FSP support . please help us to create a lpddr4x_timing.c file for our custom board , and how to use DDR config tool to create lpddr4x_config.c file to add custom board settings on DDR config tool?

Labels (1)
0 Kudos
Reply
4 Replies

1,079 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

This can be done through DDR tool in Config Tools for i.MX. You need to enter your memory features and this will generate a initialization/timing script for DDR configuration. If you need to change some register value, you can do it in this generated scripts.

Config Tools for i.MX Applications Processors | NXP Semiconductors

Here you can consult more information about how to use the tool:

User Guide for Config tools for i.MX

And here how to implement it in software in section 4.5 Building u-boot image:

MScale DDR tool

Best regards.

0 Kudos
Reply

1,074 Views
arka
Contributor III

Hi jorge,

We need to use User Guide for Config Tools for i.MX
this link document to create lpddr4x_timing.c file , in which section we need to refer,

We have our custom board yocto build, we need to add FSP support on lpddr4x_timing.c file, adding two FSP support on IMX93.

 

Tags (1)
0 Kudos
Reply

1,057 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Please refer to section 6 DDR Tool.

With FSP are you referring to frequency set point?

Best regards.

0 Kudos
Reply

1,104 Views
arka
Contributor III

We have using IMX93 custom board.

Tags (1)
0 Kudos
Reply