how to run a MX25 program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to run a MX25 program

1,427 Views
9crkzhou
Contributor III

I'v build a .bin file with IAR

when I debug with j-link , it apears normal, the led blinks.

when I download it to Nand Flash with ATK, it failed to bootup. seems to be still a USB device(in USB download mode).

how could this happen?

Labels (1)
0 Kudos
Reply
2 Replies

1,314 Views
Yuri
NXP Employee
NXP Employee

When using J-link to load and run a led example some initialization (init script, say for memory) is provided.
Looks like such initialization is not implemented in Your code. Please try to add it. 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,313 Views
9crkzhou
Contributor III

It's the DCDHeader , the IAR code does not  have it.

how to generate this part of file ?

0 Kudos
Reply