how to program 4.6M uImage to parallel nor with MFGTool?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to program 4.6M uImage to parallel nor with MFGTool?

1,518件の閲覧回数
leeseungik
Contributor III

I try to use MFG tools. MFGtools program below 4Mbytes kernel uImage. but I can't program (to parallel nor) 4.6Mbytes uImage through MFGTools.

I need uImage partitioned 8Mbytes to /dev/mtd2 partition.

I changed parallel nor partition size than compile but It doesn't work on MFGTools.

ラベル(3)
タグ(4)
0 件の賞賛
返信
2 返答(返信)

1,345件の閲覧回数
FrankLi1z
NXP Employee
NXP Employee

Mfgtools actually download uImage to target boards.

Are you sure your mfgtools's uImage you changed run at target boards?

You can use mfgtools uImage with other rootfs to enter console to check if partition really enlarged.

0 件の賞賛
返信

1,345件の閲覧回数
leeseungik
Contributor III

there are two uImage , one uImage is in OS firmware folder and the other uImage is in files folder.

if size of uImage in files folder  is over 4MB, error occures, of cause small size of uImage works fine.

uImage in OS firmware is partitioned and have 4MB at /dev/mtd2

0 件の賞賛
返信