how to parallel program emmc of multi-boards using uuu?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to parallel program emmc of multi-boards using uuu?

978 次查看
changbaoma
Contributor IV

C:\Users\Admin>uuu.exe -lsusb
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.163-0-g7e20ea1

Connected Known USB Devices
Path Chip Pro Vid Pid BcdVersion
==================================================
1:7 MX6ULL SDP: 0x15A2 0x0080 0x0001
1:9 MX6ULL SDP: 0x15A2 0x0080 0x0001


C:\Users\Admin>uuu.exe -b emmc_all u-boot-emmc-2020.04-r0.imx imx-image.rootfs.wic.bz2
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.163-0-g7e20ea1

Success 1 Failure 0


1:7 8/ 8 [Done ] FB: done
1:9 4/ 8 [=================95%===============> ] FB: flash -raw2sparse all imx-image.rootfs.wic.bz2

C:\Users\Admin>

 

As you can see, before uuu.exe finish only one board emmc program is done.

How to let(or wait) all emmc program success ?

0 项奖励
回复
0 回复数