how to make multiple-buffer effect immediately

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to make multiple-buffer effect immediately

Jump to solution
2,816 Views
jiejia
Contributor III

bsp:linux3.0.35 cpu:imx6q. My lcd resolution is 800*600

To use multiple-buffer rendering, I set 'export FB_MULTI_BUFFER=2'.

And then I print the resolution of fb0:

xres = 800

yres = 600

var.xres_virtual = 800

var.yres_virtual = 600

I download the gpu_sdk_v1.00.gz, and execute the GLES example in the file.

And then I print the resolution of fb0:

xres = 800

yres = 600

var.xres_virtual = 800

var.yres_virtual = 1200

Why multiple-buffer no effect immediately after I set 'export FB_MULTI_BUFFER=2'?

Labels (2)
0 Kudos
Reply
1 Solution
2,612 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi jie,

You should upgrade the bsp to 3.14.28 this bsp includes the vivante drv, while 3.0.35 you have to pass it by module.

Regards

View solution in original post

0 Kudos
Reply
3 Replies
2,613 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi jie,

You should upgrade the bsp to 3.14.28 this bsp includes the vivante drv, while 3.0.35 you have to pass it by module.

Regards

0 Kudos
Reply
2,612 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi jie,

BSP 3.0.35 includes vivante driver 4.6.9 p12v and this version has some bugs regarding FB_MULTIBUFFER, I strongly recommend to update vivante 5.0.11p6 included in BSP 3.14.28

Regards

0 Kudos
Reply
2,612 Views
jiejia
Contributor III

Hi Bio_TICFSL

Should I update the vivante_drv.c and vivante_drv.h?  Or,I have to update the kernel to 3.14.28?

Regards

0 Kudos
Reply