how to load the kernel thorugh nfs by using FEC0 in imx25 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to load the kernel thorugh nfs by using FEC0 in imx25 board

2,025 Views
gurumoorthirasi
Contributor IV

Dear All,

I am using imx25 board loading kernel through nfs by using debug board.

i need to load the kernel through nfs by using FEC0 on board eth adapter .

i can able to load the uImage by using FEC0 adapter. the main problem is while Os loading it is asking for DHCP Request... like below.

my uboot arg is setenv bootargs_nfs 'setenv bootargs ${bootargs} root=/dev/nfs ip=${ipaddr} nfsroot=${serverip}:${nfsrootfs}'

and i have set the ip also . but it wont take while loading ...

MX25 U-Boot > run bootcmd_nfs

Usage:

MMC sub system

MMC Device -2139095040 not found

## Booting kernel from Legacy Image at 80100000 ...

   Image Name:   Linux-2.6.31-207-g7286c01

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2113936 Bytes =  2 MB

   Load Address: 80008000

   Entry Point:  80008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux..............................................................................................

Linux version 2.6.31-207-g7286c01 (gru4cob@COB417151VM) (gcc version 4.1.2) #1 PREEMPT Mon Oct 7 15:48:31 IST 203

CPU: ARM926EJ-S [41069264] revision 4 (ARMv5TEJ), cr=00053177

CPU: VIVT data cache, VIVT instruction cache

Machine: Freescale MX25 3-Stack Board

Memory policy: ECC disabled, Data cache writeback

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 16256

Kernel command line: console=ttymxc0,115200 root=/dev/nfs ip=10.169.42.100 nfsroot=$1{serverip}:/rootfs_mount/ro3

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory: 64MB = 64MB total

Memory: 60272KB available (3940K code, 458K data, 128K init, 0K highmem)

NR_IRQS:272

MXC IRQ initialized

Clock input source is 24000000

Console: colour dummy device 80x30

Calibrating delay loop... 199.06 BogoMIPS (lpj=995328)

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

regulator: core version 0.5

NET: Registered protocol family 16

AIPS1 VA base: 0xfc000000

CPU is i.MX25 Revision 1.0

MXC GPIO hardware

Using SDMA I.API

MXC DMA API initialized

bio: create slab <bio-0> at 0

SCSI subsystem initialized

CSPI: mxc_spi-0 probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

MXC I2C driver

NET: Registered protocol family 23

regulator: REG1_BKLT: 4500 <--> 5500 mV

regulator: REG2_CPU: 2640 <--> 3877 mV

regulator: REG3_CORE: 1160 <--> 1703 mV

regulator: REG4_DDR: 1440 <--> 2115 mV

regulator: REG5_PERS: 2640 <--> 3877 mV

mc34704 0-0054: Loaded

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

Bus freq driver module loaded

Registering the CPLD Driver

3-Stack Debug board detected, rev = 0x3000300

usb: Host 2 host (serial) registered

usb: DR OTG registered

usb: DR host (utmi) registered

usb: DR gadget (utmi) registered

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.

msgmni has been set to 117

io scheduler noop registered

io scheduler anticipatory registered

io scheduler deadline registered

io scheduler cfq registered (default)

MXC Backlight Device mxc_lcdc_bl.0 Initialized.

Console: switching to colour frame buffer device 80x30

mxc_sdc_fb mxc_sdc_fb.0: fb0: DISP0 BG fb device registered successfully.

mxc_sdc_fb mxc_sdc_fb.0: fb1: DISP0 FG fb device registered successfully.

Serial: MXC Internal UART driver

mxcintuart.0: ttymxc0 at MMIO 0x43f90000 (irq = 45) is a Freescale i.MX

console [ttymxc0] enabled

mxcintuart.1: ttymxc1 at MMIO 0x43f94000 (irq = 32) is a Freescale i.MX

brd: module loaded

loop: module loaded

vcan: Virtual CAN interface driver

Freescale FlexCAN Driver

CAN device driver interface

sja1000 CAN netdevice driver

FEC Ethernet Driver

eth%d: enable RMII gasket

fec: PHY @ 0x1, ID 0x20005ce1 -- unknown PHY!

MXC MTD nor Driver 2.0

MXC MTD nand Driver 2.5

NAND device: Manufacturer ID: 0xec, Chip ID: 0xd5 (Samsung NAND 2GiB 3,3V 8-bit)

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

uncorrectable error :

nand_bbt: ECC error while reading bad block table

Searching for RedBoot partition table in NAND 2GiB 3,3V 8-bit at offset 0x7fec0000

No RedBoot partition table detected in NAND 2GiB 3,3V 8-bit

Creating 5 MTD partitions on "NAND 2GiB 3,3V 8-bit":

0x000000000000-0x000000300000 : "nand.bootloader"

0x000000300000-0x000000800000 : "nand.kernel"

0x000000800000-0x000010800000 : "nand.rootfs"

0x000010800000-0x000011000000 : "nand.configure"

0x000011000000-0x000080000000 : "nand.userfs"

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

MXC keypad loaded

input: mxckpd as /class/input/input0

Linux video capture interface: v2.00

Driver for 1-wire Dallas network protocol.

PMIC Character device: successfully loaded

i.MX ADC at 0x50030000 irq 46

mxsdhci: MXC Secure Digital Host Controller Interface driver

mxsdhci: MXC SDHCI Controller Driver.

mmc0: SDHCI detect irq 161 irq 9 INTERNAL DMA

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.20.

regulator: Unable to get requested regulator: VDDD

sgtl5000-i2c 0-000a: SGTL5000 revision 17

No device for DAI imx-ssi-1-0

No device for DAI imx-ssi-1-1

No device for DAI imx-ssi-2-0

No device for DAI imx-ssi-2-1

DMA Sound Buffers Allocated:UseIram=1 buf->addr=78001000 buf->area=c4900000 size=65536

DMA Sound Buffers Allocated:UseIram=1 buf->addr=83ab0000 buf->area=fdf2e000 size=65536

asoc: SGTL5000 <-> imx-ssi-1-0 mapping ok

mmc0: new high speed SDHC card at address e624

mmcblk0: mmc0:e624 SU04G 3.69 GiB

mmcblk0: unknown partition table

ALSA device list:

  #0: imx-3stack (SGTL5000)

oprofile: using timer interrupt.

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

can: broadcast manager protocol (rev 20090105 t)

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

smsc911x: Driver version 2008-10-21.

smsc911x-mdio: probed

eth1: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)

net eth1: MAC Address: 00:04:9f:00:f6:21

Static Power Management for Freescale i.MX25

regulator_init_complete: incomplete constraints, leaving REG5_PERS on

regulator_init_complete: incomplete constraints, leaving REG1_BKLT on

input: imx_adc_ts as /class/input/input1

i.MX ADC input touchscreen loaded.

drivers/rtc/hctosys.c: unable to open rtc device (rtc0)

eth0: enable RMII gasket

net eth1: SMSC911x/921x identified at 0xc48fc000, IRQ: 256

Sending DHCP requests ....�

Please someone will help on this where i need to change to load the kernel through nfs by using FEC0 of imx25 personality board ASAP.

Regards,

Guru

Labels (2)
0 Kudos
Reply
2 Replies

1,546 Views
Yuri
NXP Employee
NXP Employee

Looks like there is no DHCP server for i.MX25. Please try to use a (local) router to connect i.MX25 board and NFS server.

Another solution - to use static IP (in the same subset as the NFS server) for i.MX25.

0 Kudos
Reply

1,546 Views
gurumoorthirasi
Contributor IV

hi Yuri,

I am using static ip only .. but i didnt take . but it is fine if i use debug board adapter

Please tel what exactly should i do to disable dhcp and to enable from our static ip.

this is high priority!!

Regards,

Guru

0 Kudos
Reply