how to know the keyboard driver is installed or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to know the keyboard driver is installed or not?

1,069件の閲覧回数
freescaleusr1
Contributor I

Hi,

now my lcd panel can get displayed after boot. I can use uart console to input command in console shell, i think to know if the keyboard driver get installed so that i plug keyboard to directly input command on screen, i input "dmesg | grep keyboard" and get nothing, so how to know keyboard driver get installed or not? (I use core-image-minimal yocto image).

looking forward to reply, thanks.

ラベル(3)
0 件の賞賛
返信
1 返信

952件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello wz ca,

The keyboard driver is enabled on the core-image-minimal image of the i.MX BSP. However, you may not see the driver enabled until you insert a USB keyboard (make sure to use a USB OTG cable to connect the keyboard).

I hope this helps!

0 件の賞賛
返信