how to interface an 18bit-RGB display to iMX6SL kitkat4.4.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to interface an 18bit-RGB display to iMX6SL kitkat4.4.2

885件の閲覧回数
jansirani
Contributor III

Hello everyone,

we have a custom board using  iMX6SL with Android 4.4.2.

In our custom board previously we interfaced successfully  7inch display in RGB24bit .

Now we have to interface a 2.8 inch display which supports 18bit RGB format only.

Please tell us what are the changes we have to do in BSP in order to interface a 18bit RGB display to our custom board.

Thanks,

D.Jansirani

1 返信

769件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Jansi,

RGB18 is not supported, for MX6SL Configurable are: RGB 16, 24 or 32 bits per pixel frame buffer

Regards