how to fetch and compile 6.6.1 kernel version of imx using toolchain

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to fetch and compile 6.6.1 kernel version of imx using toolchain

784 Views
srinivas_123
Contributor III

i am using imx8mplus lpddr4 evk .i am building toolchain for imx8mplus using yocto .

i am using IMXLXYOCTOUG v.LF6.6.3_1.0.0 BSP of the Yocto user guide .

i build SDK using

 bitbake  core-image-minimal  -c  populate_sdk

environment setup for toolchain

source /opt/fsl-imx-xwayland/6.6-nanbield/environment-setup-armv8a-poky-linux

 export ARCH=arm64

clone the kernel

git clone https://github.com/nxp-imx/linux-imx -b lf-6.6.y
cd linux-imx

make imx_v8_defconfig
make

it generates the kernel image and dtb files. so i copied these files into sd card and boot up the board .

while  booting  it shows the  kernel version of 6.6.23_2.0.0 but i need 6.6.3_1.0.0

could anyone knows , please help me .i want to customize the 6.6.3.1.0.0 kernel , i have to reduce the kernel size and remove the unwanted module .
But the above following steps takes 6.6.23_2.0.0 version and size of kernel is more .how to fetch the 6.6.3_1.0.0 and compile and reduce the size .

Thanks &regards

Srinivas

0 Kudos
Reply
1 Reply

748 Views
Harvey021
NXP TechSupport
NXP TechSupport
0 Kudos
Reply