how to enable rs485 in imx53 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to enable rs485 in imx53 board

1,532 次查看
yennivenkateswa
Contributor II

Hi all,

presently, i am using imx53 board its baurdrate is 115200 and its rs232 communication. but i want rs485 communication and baurdrate is 460800

anyone please help me how can i enable rs485 communication with that baurdrate ?

Thanks&Regards

Venkatesh

0 项奖励
回复
1 回复

1,177 次查看
Yuri
NXP Employee
NXP Employee

Strictly speaking, the i.MX53 does not fully support the RS-485 in hardware.

Traditionally the RTS is used to control transfers, since UART activates RTS at

when data is available to transmit, and a UART checks CTS before and during the

transmission of the data. When all data has been transmitted, the UART should

deactivate RTS.

   Some issues may occur because of fact, that RTS control bits relate to FIFO

activities, and does not control RTS fully correctly for RS-485. Additional

software is needed to check when all data bits are really sent to line.

   Also, there are a lot RS232-RS485 automatic converters. These converters contains

a fast automatic TX enable circuit. Please look at the following :

http://www.rs485.com/pasc24t.html

http://www.tri-plc.com/auto485.htm

http://www.tri-plc.com/documents/inst-auto485.PDF

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复