how to disable the configuration option FB_MXC_VAR_WVGA_SYNC_PANEL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to disable the configuration option FB_MXC_VAR_WVGA_SYNC_PANEL

1,169件の閲覧回数
sarathithiru
Contributor I

I am using Imx 6 pico sbc with linux 3.035. i have interfaced my board with LVDS. but i am getting the screen as attached below.

screens are splitted in to 6 views

please get me some solution to solve this.

IMG_20151014_152242497.jpg

Regards

sarathi.T

ラベル(3)
2 返答(返信)

1,100件の閲覧回数
Aubineau_FAE
NXP Employee
NXP Employee

Hi,

What is the resolution of your screen and what is the resolution of your framebuffer?

Does it match?

if not can you try the fbset command, for instance:

fbset -fb /dev/fb0 -g 1024 768 1024 2304 32

check resolution, fb number and bpp.

check also fbset manual:

fbset - Linux Command - Unix Command

BR

V.

1,100件の閲覧回数
sarathithiru
Contributor I

i have rectified this error, by changing the display standard.

Thank you

0 件の賞賛
返信