how to check CCM IOMUXC etc value after kernel boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to check CCM IOMUXC etc value after kernel boot.

1,518 Views
lifusong
Contributor IV

As the title.

any body have good ideas?

thanks.

Labels (2)
0 Kudos
Reply
4 Replies

1,394 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

one can try memtool for read/write registers:

http://cache.freescale.com/files/32bit/doc/app_note/AN4576.pdf p.30

android-imx6-kitkat/0400-ENGR00268294-Add-memtool-test-into-i.MX6-android.patch at master · rabeeh/a...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,394 Views
lifusong
Contributor IV

Hi,sir.

  thanks for your help.

how to add the memtool into android 4.4.3_r1 kernel 3.10.53 ?

thanks very much

0 Kudos
Reply

1,394 Views
lifusong
Contributor IV

Dear igorpadykov

     thanks for you help.

  does there have  Power Consumption Measurement datasheet for IMX6Q?

0 Kudos
Reply

1,394 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

Application Note AN4509 (Rev. 0, 10/2012) "i.MX 6Dual/6Quad Power Consumption Measurement"

http://www.freescale.com/files/32bit/doc/app_note/AN4509.pdf

0 Kudos
Reply