how to check Bluetooth from an androidized kernel?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to check Bluetooth from an androidized kernel?

1,521 Views
abraham_v
Contributor IV

Hello,

I have a custom board built around the iMX6 dual core processor. It's running android version 4.2 and has a wl1271 chipset connected (for wifi and bluetooth). The bluetooth interface is via UART.

Theoretically, the pin multiplexing has been done and UART initialized. But does anyone know how the bluetooth module could be tested/probed from linux command line? As for android 4.2, google has shifted to using the "bluedroid" libraries and I'm not sure what application could be used in conjunction with this to test the module.

Puzzled,

Abraham V.

PS: I know this is not an iMX6 question, but I'm not sure where else to ask.

Labels (4)
Tags (3)
0 Kudos
Reply
0 Replies