how to change read/write latency of dram on imx93evk?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to change read/write latency of dram on imx93evk?

2,230 次查看
jekim
Contributor IV

Hello,

 

I'm using the imx93evk. The default dram configurations can be automatically generated by config tool per clock frequency selection. btw, increasing/decreasing the read/write latency is not supported by the config tool. I tried to directly change the lpddr4x_timing.c file to increase the latency. (RL 36 to 40, WL 16 to 18) The two c files are attached. TIMING_CFG_1, TIMING_CFG_2, TIMING_CFG_3, and MR2 register are modified on the new file. However, the u-boot failed with the message of "Malloc buffer failed". please let me know how to achieve this condition change.

 

Thanks.

0 项奖励
回复
2 回复数

2,228 次查看
pengyong_zhang
NXP Employee
NXP Employee

Hi @jekim 

You can follow the bwlow picture set your WL RL.

pengyong_zhang_0-1718181982009.png

ps : We do not suggest customer modify this parameters , different value follow the different  DDR frequency and mode.

B.R

0 项奖励
回复

1,579 次查看
jekim
Contributor IV

Hi @pengyong_zhang ,

 

It is required to change the latency at a clock frequency for the failure analysis. Is it impossible or too complicated?

 

Thanks.

0 项奖励
回复