how to change csi_id to 1 from 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to change csi_id to 1 from 0

910 Views
srinivasaporam
Contributor II

Hi,

I have got a Wandboard dual/Quad. I have downloaded 3.10.53 from the git hub and made the the board to ow we are connecting the Raspi camera (ov5647) to this board. Raspi camera is using IPU-1 and CSI-1 (ipu_id=<0> and csi_id=<1>). But where as wandboard is using IPU-1 and CSI-0 (ipu_id=<0> and csi_id=<0>). How can i change this csi_id used by wandboard to 1 from 0, so that  ov5647 sensor will work.

If i change this in dts file will it be ok or i need to change in kernel source files. if i need to change in kernel souces files, which are those files????? kernel is 3.10.53

0 Kudos
Reply
1 Reply

802 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

changing dts file should be ok no need to change source files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply