how to build filesystem without build the kernel image in yocto

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to build filesystem without build the kernel image in yocto

3,317 次查看
huyongfa
Contributor II

now i'm blocked by the following error inyocto, when build fsl-image-gui, the do_fetch always be failed.

WARNING: Failed to fetch URL git://git.freescale.com/imx/linux-2.6-imx.git attempting MIRRORS if available.

i have my own kernel image, and don't need bo build this kernel image.

1. so is there some way to build a filesystem without build the kernel image?

i have tried specify the path of my own kernel in linux-imx_3.14.52.bb, but is always failed at do_configure.

4 回复数

3,170 次查看
BiyongSUN
NXP Employee
NXP Employee

Suggest for the Yocto questions, you can check the Yocto project.

If you check the yocto document you can find the command.

http://www.yoctoproject.org/docs/2.2/mega-manual/mega-manual.html

Untitled.png

also you can find in the task list.

do_package_setscene            Analyzes the content of the holding area and splits it into subsets based on available

...........

.......
do_rootfs                        Creates the root filesystem (file and directory structure) for an image
do_unpack                      Unpacks the source code into a working directory
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and all succeeded.
bysun@imx-fae-server-sh:~/yocto/L4.1.15-1.1.0_ga/fsl-release-bsp/imx6ulevk$

3,170 次查看
huyongfa
Contributor II

after a long wait, now i have passed yocto kernel building, rootfs also is ready.

your respones is very usefull, i will try it later.

many thanks to you.

0 项奖励
回复

3,170 次查看
Yuri
NXP Employee
NXP Employee

Hello,

   I think, hardly this is possible and makes sense to build system without kernel built.

Regards,

Yuri.

0 项奖励
回复

3,170 次查看
huyongfa
Contributor II

it is very usefull for me, because it is need a very long time to git kernel source from git.freescale.com.

and this kernel is not needed for me,as i have my own kernel.

0 项奖励
回复