how to application u-boot command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to application u-boot command

1,414 Views
kangmw086
Contributor III

hi

i used i.mx6 sabreauto board.

Is it possible to add / remove / modify u-boot command in application after I.MX6 board booting is completed?
I want to create a linux application that will function like 'setenv ~~', 'saveenv' in the u-boot menu when booting the board.
Do you have references or examples?

And is there a way to control it like gui instead of command in u-boot like windows cmos?
It does not have to be 'gui'. You need something to select the u-boot command.

regards!!

Labels (2)
0 Kudos
Reply
1 Reply

1,349 Views
igorpadykov
NXP Employee
NXP Employee

Hi k

as this is specific uboot question one can post it to uboot mail list

U-Boot Info Page 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply