how imx8mm evk platform ddr4 calibrate?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how imx8mm evk platform ddr4 calibrate?

Jump to solution
1,014 Views
jxingyang
Contributor I

HI ALL

I am study the ddr4 calibrate steps now, and have some confuse for ddr4 calibrate with following link.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

From the MSCALE_DDR_Tool_User_Guide.pdf,  it seems that the target platform didn't need run any sd card image when ddr4 calibrate, why MSCALE_DDR_Tool.exe can download the bin file to the target?

regards

jason

0 Kudos
Reply
1 Solution
984 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @jxingyang 

 Because for DDR calibration part. only need run the DDR firmware is OK. do not need full iamge.

View solution in original post

0 Kudos
Reply
3 Replies
948 Views
pengyong_zhang
NXP Employee
NXP Employee

all of these  .bin files will be downloaded.

0 Kudos
Reply
985 Views
pengyong_zhang
NXP Employee
NXP Employee

hi @jxingyang 

 Because for DDR calibration part. only need run the DDR firmware is OK. do not need full iamge.

0 Kudos
Reply
983 Views
jxingyang
Contributor I

I means that when run the MSCALE_DDR_Tool.exe tool,my platform didn't run any image,  the download log as follow:

Downloading file 'bin\lpddr4_train1d_string_v201709.bin' ..Done

Downloading file 'bin\lpddr4_train2d_string_v201709.bin' ..Done

Downloading file 'bin\lpddr4_imem_1d_v201709.bin' ..Done

Downloading file 'bin\lpddr4_dmem_1d_v201709.bin' ..Done

Downloading file 'bin\lpddr4_imem_2d_v201709.bin' ..Done

Downloading file 'bin\lpddr4_dmem_2d_v201709.bin' ..Done

Downloading IVT header...Done
Downloading file 'bin\m845s_ddr_stress_test.bin' ...Done

Download is complete
Waiting for the target board boot...

so which one use the usb port download the bin files?

0 Kudos
Reply