how do I configure the i2c host with clock stretching ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how do I configure the i2c host with clock stretching ?

Jump to solution
3,705 Views
Luke-Hsieh
Contributor III

I'm trying to have TI gauge bq27542-g1 worked on imx8m nano EVK with pure Linux OS.

I was aware that i2c host must support i2c clock stretching to wait for slow slave response.

 

Can anyone share your experience any specific change in DTS or in the driver to support i2c clock stretching ?

 

 

0 Kudos
Reply
1 Solution
3,693 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luke

 

it is supported in hardware as described in sect.15.1.3.5 Clock stretching, no additional

dts settings are needed   i.MX 8M Nano Applications Processor Reference Manual

 

Best regards
igor

View solution in original post

2 Replies
3,682 Views
Luke-Hsieh
Contributor III

Hi Igor,

 

Thanks for the confirmation!

I will give it a try when I receive the device which is a fuel gauge IC.

0 Kudos
Reply
3,694 Views
igorpadykov
NXP Employee
NXP Employee

Hi Luke

 

it is supported in hardware as described in sect.15.1.3.5 Clock stretching, no additional

dts settings are needed   i.MX 8M Nano Applications Processor Reference Manual

 

Best regards
igor